Discontinued in the end of September 2018.
Only click one of the "Agree" buttons and begin downloading if you accept the above license agreement.
Discontinued in the end of September 2018.
Discontinued in the end of September 2018.
Operating System | 32bit (x86) : Microsoft Windows XP(SP3), Vista(SP2), 7 64bit (x64) : Microsoft Windows XP x64 Edition(SP2), Vista(SP2), 7 |
---|---|
Microsoft.NET Framework | Any one of 4/4.5 |
Hard-Disk Space | A capacity of 1.5GB or more is preferable (NOT include .NET Framework) |
Others | Administrator authority is required for installation. |