Contact

FAQ

Q.ESR characteristics (6): What should be taken into consideration when the ESR is a critical parameter in a circuit design?

Capacitors >  Ceramic Capacitors >  Multilayer Ceramic Chip Capacitors

A. If ESR is a critical parameter for the operation of a circuit, then the design engineer needs to consider two parameters. The first parameter is the operating frequency of the circuit. The second parameter is the overall temperature of the component which includes the external temperature around the component as well as the internal self-heating due to current level.


>>Multilayer Ceramic Chip Capacitors Product Site

For any other product-related questions or inquiries, please contact us throughone of our sales representatives or this website.

Has this FAQ been useful? YesNo

All related FAQ