Tech Library
Application & Cases
[ ]
Application Note

Product Development Utilizing TDK's Proprietary Pattern Coil Technology

TDK, as part of its continued efforts to bring environmentally friendly technical solutions to the market, has recently developed a plating process that enables manufacturing of thick, highly precise copper patterns on thin-film substrates without using typical exposure/etching technologies. The copper deposition can be to one or both sides of the thin-film substrate to reduce the coil’s [antenna’s] DC resistance (DCR). This innovation has been achieved through an electro-plating process that uses a nano-dispersed organic polymer called polypyrrole (PPy), a material solution from Achilles Corporation and is combined with TDK’s internal process technology. TDK’s unique copper plating process employs an "additive” methodology, where copper is plated only on defined areas to form the required pattern and is in direct contrast to standard methods that etch away from a copper layer in a subtractive process. Additionally, by incorporating TDK’s proprietary high-performance magnetic shielding materials, end-product miniaturization can be realized.

Product Lineup of Pattern Coils

TDK's proprietary pattern coil technology allows for precise and flexible adjustments to the thickness of copper traces based upon application requirements. This capability enables highly customizable coil designs that are not achievable with conventional copper coil technologies such as those created by etching. The end-product lineup includes: coils/antennas for Wireless Power Consortium (WPC) Qi standard wireless power transfer (WPT) coils, antennas for the AirFuel standard of WPT, other non-Qi standard WPT coils, RFID/NFC antennas for both communication and power, and EMI mesh screens. Further thickness reduction can be achieved by embedding the copper antenna into the adhesive layer used to adhere the antenna to its magnetic shield, where the shield is used to contain the magnetic flux (Ø) of the magnetic field (H). These capabilities facilitate the use of patterns coils in a wide variety of end applications. Typical copper thickness versus end application information is shown in Figure1.

Figure 1: Typical Copper Thickness vs. End Application

TDK Ultra-Thin NFC Antenna MSC Series

NFC communication, used for contactless payments, secured access, and personal authentication, requires a magnetic resonance loop antenna. However, communication can be hindered by nearby metal environments, so a combination of an antenna plus a magnetic shield may be necessary.
As NFC-equipped devices become smaller and lighter, the integrated loop antennas also need to be smaller and/or thinner, which can create challenges for traditional antenna technologies. This is highlighted in Figure 2.
TDK's pattern coil NFC antennas make use of TDK’s magnetic shield manufacturing technology to embed the antenna into the adhesive layer attached to the magnetic shield, thus achieving further antenna thickness reduction. Additionally, optimizing the design with the best magnetic material maximizes performance and enables even thinner magnetic sheets.
The NFC Forum has also released a standard where NFC antennas and frequencies are used to wirelessly charge low power devices like wearables. The pattern coil’s antenna configuration flexibility is advantageous when small antenna sizes and/or irregular shapes are required due to the physical dimensions of the low power to-be-charged device.

Figure 2: Thin and Lightweight Single-Pattern Coil

Ultra-Thin Permalloy Sheet IPM Series

Electromagnetic interference [EMI] noise suppression within electronic devices is essential for ensuring proper operation and compliance with regulatory standards. However, It can be difficult to completely suppress unwanted noise in circuit design, and shielding materials are often used as a countermeasure against both conducted and radiated noise.
 Inexpensive metal cases are often used as shielding materials, but while they are effective for high-frequency noise, they are less effective for low-frequency noise, and the thickness of the case must be increased to achieve the necessary shielding performance.
 The IPM series is an ultra-thin soft magnetic metal sheet, and the use of Permalloy, a high magnetic permeability material, dramatically increases its effectiveness against low-frequency noise, and below 500 kHz, it shows shielding performance equivalent or superior to that of a stainless steel plate which is 100 times thicker.
 A single magnetic layer version of the IPM01 series is shown in Figure 3.

Figure 3: TDK’s IPM Magnetic Shield Series

IPM Series Applications

With the continued miniaturization, thinning, and multi-functionality of electronic devices, EMI noise suppression in smartphones and other electronics has become increasingly important. TDK’s IPM01 series offers leading-edge high permeability magnetic materials, with an integrated copper layer therefore optimizing EMI noise suppression in various electronic devices and in applications featured in Figure 4. TDK’s IPM01 material is available on rolls, in sheet format, and in custom sizes and shapes. A heat-resistant design, capable of operating in environments up to 125°C, is currently in development and is scheduled for mass production in 2025.

Figure 4: Examples of IPM Series Applications
contact-us

For inquiries related to our products or sales, please contact us by filling the following Contact Form.

Contact Form

Please click here for information on the list of distributors.

Related Links