Application Note Devices that Enhance the Safety of the Digital Cockpit
- PowerHap Actuator Product Portal
- MEMS Microphone Product Portal
- Ag-Stacked Transparent Conductive Film Product Portal
The automobile industry is developing the digital cockpit in pursuit of an HMI that will provide safety and reassurance while freeing drivers from the burdens of driving and allowing time to be used meaningfully and in comfort.
Below is an introduction to TDK products and technologies that enhance the value of the digital cockpit to achieve an HMI that ensures and enhances safety and reassurance through the driver's senses.
Contents
- The digital cockpit will determine the product value of next-generation automobiles
- Piezo actuators convey tactile sensations and the feel of operation
- MEMS microphone eliminates road noise and enables reliable voice operation
- Ag-stacked transparent conductive film provides electrical functions to the car windows
- Contact
- Related Links
The digital cockpit will determine the product value of next-generation automobiles
The cockpits of current automobiles are equipped with an instrument panel that shows the speedometer, tachometer, fuel gauge, water temperature gauge, trip meter, and other information necessary for driving as well as display devices that support the driver such as center information displays that show navigation maps and so on.
The digital cockpit will spur a shift from conventional analog meters to liquid crystal displays, and it is thought that it will be possible to switch between travel information useful to passengers during autonomous driving and information that supports driver operation during manual driving by a driver shown on the same large screen.
Relying solely on the visual appeal of the display, however, cannot achieve both safety in transportation and convenience and comfort.
Achieving level-3 automated driving requires rapid handover of responsibility for driving operations from the system to the driver when driving becomes difficult (Table 1).
This chapter presents TDK Group products and technologies that link cars and humans to provide sensory information other than visual.
| Driving Mode | SAE Level | Driving Operations |
|---|---|---|
| Full automation | Level 5 | ・The system performs all operations (no limitation on areas) ・The system responds even during emergencies and when the system operation is difficult |
| High automation | Level 4 | ・The system performs all operations in certain areas (highways, etc.) ・The system responds even during emergencies and when the system operation is difficult |
| Conditional automation | Level 3 | ・The system performs all operations in certain areas (highways, etc.) ・The driver responds even during emergencies and when the system operation is difficult |
| Partial automation | Level 2 | ・The system supports both steering and acceleration/deceleration |
| Driver assistance | Level 1 | ・The system supports either steering or acceleration/deceleration |
| No automation | Level 0 | ・The driver performs all operations |
Piezo actuators convey tactile sensations and the feel of operation
If an HMI should convey not only visual but also tactile information, it will be possible to enhance the feel of operating devices and the sense of realism when using infotainment functions. TDK's PowerHap piezo actuators can provide clear tactile responses to drivers. They can be made thinner than electromagnetic actuators, which makes it possible to embed them in small spaces such as a steering column. In addition, PowerHap piezo actuators have excellent responsiveness, start-up rapidly when vibrating, and can create diverse vibration patterns to generate tailored sensations. Moreover, they generate voltage when force is applied, so they can be used in conjunction with pressure sensors, which are input devices.
TDK is working with Boréas Technologies Inc. by collaborating on the company's piezo actuator drive ICs to provide solutions that enable developments to faithfully create freely designed tactile patterns.
| Piezoelectric | Electromagnetic | |
| PowerHap | ERM, LRA | |
| Thickness [mm] | 1.2 - 2.4 | 3 |
| Acceleration [g] / 20 g mass | 8 - 65 | 2 - 5 |
| Rapid start-up [ms] | < 1 | 20 - 50 |
| Voltage [V] | 60 / 120 | 3 |
| Unrestricted waveform design | Yes | No |
| Pressure sensitivity | Yes | No |
・Since the actuators are thin, they support flexible designs for all types of devices.
・Rapid start up and unrestricted vibration design
* ERM and LRA support only sine wave design.
MEMS microphone eliminates road noise and enables reliable voice operation
Voice Recognition is a key component in the digital cockpit. Equipped with numerous microphones, this will enable the operation of onboard devices, such as air conditioning, and be used with voice communications. While driving the interior space is filled with various noises such as wind, traffic. and the motor itself. To ensure reliable audio capture under these conditions, the use of enhanced performance microphones suitable for noise canceling and voice capture technology is needed.
TDK's MEMS microphones can fulfill the technological requirements for automobile interior environments. The ICS-40730 features the world's highest signal-to-noise (S/N) ratios at 74dBA the INMP621. it is possible to realize a directional microphone system in automobile interior environments easily. because a directional algorithm is added that uses a digital interface of pulse density modulated (PDM) linked with two microphones to be time multiplexed on a single data line. The MMICT4078-00-908 has an acoustic overload point (AOP) of 135dBA, which is great for listening in noisy environments, and the ICS-40300’s low-frequency response makes it an excellent choice for precise phase matching.
By incorporating these microphones into various sites in the vehicles interior, it is possible to selectively capture the voice of speakers at specific locations, and to listen and cancel out obtrusive noises, making the digital cockpit a key selling point of the vehicle.
| Product number | ICS-40730 | INMP621 | MMICT4078-00-908 | ICS-40300 |
|---|---|---|---|---|
| Product image | ||||
| Product type | Analog output | Digital output | Analog output | Analog output |
| Dimensions (L x W x T) [mm] | 4.72 x 3.76 x t:3.5 | 4 x 3 x t:1 | 3.35 x 2.5 x t:0.98 | 4.72 x 3.76 x t:3.5 |
| S/N ratio [dBA] | 74 | 65 | 66 | 63 |
| AOP [dBA] | 124 | 133 | 135 | 130 |
* Please use MEMS microphones after confirming the product operating temperature and using a microphone within its guaranteed range. Contact TDK for details.
Ag-stacked transparent conductive film provides electrical functions to the car windows
A smart and stylish digital cockpit can be created by adding electrical functions to the front, rear, and side windows and the surfaces of information displays. By adopting TDK's Ag-stacked transparent conductive films, which feature both high transparency and low resistance and are also flexible, we are enabling applications such as light control film (our product used as an electrode) and functional enhancement of glass surfaces to serve for example as touch sensors, antennas, or anti-condensation film heaters (our product used as an element of functional films). The surface resistance is 10 Ω/sq., lower than that of ITO, which is widely used as a transparent electrode material. As a result of these outstanding characteristics, the films can contribute to creating practical and attractive vehicle interiors.
| Structure | Type A | Type B |
|---|---|---|
| Material | PET | PET |
| Surface resistance [Ω/sq.] | 10 | 4 |
| Total light transmittance [%] | 87 | 82 |
| Haze [%] | 0.5 | 0.5 |
| b* (Yellow tint) | 2.5 | 5.5 |
Contact Information
Related Links
Product Portals
- PowerHap Actuator Product Information
- A comprehensive guide to various information concerning TDK Group's PowerHap actuators.
- MEMS Microphone Product Information
- A comprehensive guide to various information concerning TDK Group's MEMS microphones.
- Ag-Stacked Transparent Conductive Film Product Information
- A comprehensive guide to various information concerning TDK Group's Ag-Stacked Transparent Conductive Films.