FAQ
Q.
What is “amplitude permeability μa”?
  • Ferrite und Zubehör
  • >
  • Ferrite-Kerne



A. It is the relative permeability acquired from the maximum value of the magnetic flux density and the maximum value of the intensity of the magnetic field when there are periodic changes in a magnetic core that is in a demagnetized state and a magnetic field that makes the average value of the intensity “zero” is applied.

* Terminology related to ferrites can be found in the website in ”Terms Definitions and Explanations” under ”Ferrite Summary”.
* The symbol and the catalog of this data are in accordance with IEC Publication 60401-3.
* Our terminology and settings were established by reference to JIS C 2560-1,-2.