FAQ
Q.
Measurements of SRF (7): What will happen if I do not compensate for the short chip inductance of an impedance analyzer?
  • Capacitors
  • >
  • Multilayer Ceramic Chip Capacitors


A. When the meter is compensating the short chip, meter will assume the short chip has 0 inductance. But the truth is that the short chip does have some parasitic inductance. When the compensation performed, the parasitic inductance will be compensated as part of the fixture parasitic. As the result, the meter has the offset of parasitic inductance. Once the short chip parasitic inductance becomes a part of the parasitic of the fixture, the parasitic of the gold short chip will always present. Therefore, ESL of the DUT will be lower due to the parasitic short chip inductance and thus higher SRF readings. (see Figure 1)*.

Once the short chip inductance is compensated, the measurement of the SRF will be the true data (see Figure 2).


Figure 1: Zero inductance compensated; lower ESL thus higher SRF.

Figure 2: The true SRF measurement of the capacitor.
* TDK MLCC Application Notes, “MLCC Measurement Procedure for |Z| and ESR vs. Frequency”, M.Waldrip (1999)


>>Multilayer Ceramic Chip Capacitors Product Site

For any other product-related questions or inquiries, please contact us throughone of our sales representatives or this website.