FAQ
Q.
What is the zero load resistance value?
  • Voltage / Current / Temperature Protection Devices
  • /
  • Sensors and Sensor Systems
  • >
  • Temperature Protection Devices
  • /
  • Temperature Sensors (NTC)
  • >
  • Chip NTC Thermistors (Protection Device)
  • /
  • Chip NTC Thermistors (Sensor)


A. Resistance value of a thermistor measured at a prescribed temperature, also called no-load resistance value.
The value is normally measured at a standard temperature of 25°C.
The measurement is conducted at a power level such that the influences of spontaneous heat generation can be negligible.