FAQ
Q.
What is the B constant?
  • Voltage / Current / Temperature Protection Devices
  • /
  • Sensors and Sensor Systems
  • >
  • Temperature Protection Devices
  • /
  • Temperature Sensors (NTC)
  • >
  • Chip NTC Thermistors (Protection Device)
  • /
  • Chip NTC Thermistors (Sensor)


A. A constant representing change in resistance, calculated using the resistance value at two specified ambient temperatures according to the following formula.

B=ln (R/R0) / (1/T-1/T0)

R: Resistance value at time when ambient temperature is T (K) R0: Resistance value at time when ambient temperature is T0 (K)