Q.
What is withstand voltage?
- Voltage / Current / Temperature Protection Devices /
- Sensors and Sensor Systems >
- Temperature Protection Devices /
- Temperature Sensors (NTC) >
- Chip NTC Thermistors (Protection Device) /
- Chip NTC Thermistors (Sensor)
A. Indicates the amount of voltage that can be resisted when applied for three minutes in still air at 25°C. Withstand voltage is measured using a method that starts at 0V and then gradually increases the amount of voltage applied.