- Capacitors >
- Multilayer Ceramic Chip Capacitors /
- MLCC with Dipped Radial Lead
A.
Mean time between failure is the arithmetic mean (or average) time between failures of a given device or system and is normally measured in hours. This statistical value is meant to represent the average amount of time that will pass between random failures for a large sample over a long period of time for a given component. It is also an indicator of system reliability that is calculated from known failure rates of various components in the system.[3,4,5]
MTBF calculations are used to predict behaviors for a large (or entire) population, not the behavior from a particular site or smaller subset of the population. Therefore MTBF only applies to the cumulative analysis of large numbers of components; it says nothing about a particular unit.[5] Figure 1 gives a visual overview of the concept.
Figure 1. MTBF Illustration.
>>Multilayer Ceramic Chip Capacitors Product site
>>MLCC with Dipped Radial Lead Product site
For any other product-related questions or inquiries, please contact us throughone of our sales representatives or this website.