- Capacitors >
- Multilayer Ceramic Chip Capacitors /
- MLCC with Dipped Radial Lead
A.
An impedance analyzer can measure the capacitance in parallel known as Cp or in series known as Cs. The circuit model will be depending on the value of capacitance of the capacitor (see Figure 1).
When C is small and impedance is high, parallel impedance between C and Rp will become significantly higher than Rs. Thus the meter setting for measuring capacitance should be Cp. When C is large and impedance is small, parallel impedance for C and Rp is not as significant. Therefore, Cs should be used for the meter setting to measure capacitance. A good rule of thumb to select the impedance setting is to use Cp for capacitor impedance values greater than 10kΩ and Cs for less than 10Ω.
Figure1: Impedance equivalment circuit
>>Multilayer Ceramic Chip Capacitors Product Site
>>MLCC with Dipped Radial Lead Product Site
For any other product-related questions or inquiries, please contact us throughone of our sales representatives or this website.